AXIS#.IL.FRICTION
Description
Position command derivative sign is multiplied by this value to be injected to the current command.
-
-
AXIS#.IL
"Instruction list"
This is a low-level language and resembles assembly.FRICTION is active in Position and Velocity modes (OPMODE = 1, 2), but not active in Torque
Torque is the tendency of a force to rotate an object about an axis. Just as a force is a push or a pull, a torque can be thought of as a twist mode (OPMODE = 0).
Versions
| Action | Version | Notes |
|---|---|---|
| Implemented | 02-00-00-000 |
General Information
|
Type |
Read/Write |
|
Units |
A |
|
Range |
0 to the minimum of user positive current limit (AXIS#.IL.LIMITP ) and motor peak current (AXIS#.MOTOR.IPEAK ). |
|
Default Value |
0 |
|
Data Type |
Float |
|
See Also |
|
|
Stored in Non Volatile Memory |
Yes |
Variants Supported
All variants are supported.
Fieldbus Information
| Fieldbus |
Parameter | Index | Sub-Index | Data Type | Float Scale | Units | Access | PDO |
|---|---|---|---|---|---|---|---|---|
| EtherCAT |
AXIS1.IL.FRICTION | 0x500A | 0xB | DINT | 1000:1 | - | RW | False |
| AXIS2.IL.FRICTION | 0x510A | 0xB | DINT | 1000:1 | - | RW | False |